AnsweredAssumed Answered

Problem with No-Os reference design for FMCOMMS2 with zedboard

Question asked by Jetmiri on Aug 6, 2014
Latest reply on Feb 6, 2015 by mochen2100@163.com

I downloaded the HDL reference design in

Using the ISE 14.6 I tried to open the hdl reference design on XPS. It updates the IP with the newer version and I started to generate the bitstream. There were some errors regarding the netlist for ip axi_dac_4d_2c_v1_00_a and adi_common_v1_00_a. I generated the netlists (.ngs fils and .v files) using the procedure described in AD-FMCOMMS1-EBZ HDL Reference Design [Analog Devices Wiki]


After the generation of bitstream I exported on EDK. I am using the SDK 2013.2.

I downloaded the No-Os reference design form the link no-OS/ad9361/sw at master · analogdevicesinc/no-OS · GitHub and imported the files on the source folder of the project as described in the link http://wiki.analog.com/resources/eval/user-guides/ad-fmcomms2-ebz/software/baremetal


The problem is that the XPAR_AXI_AD9361_0_BASEADDR and XPAR_AXI_AD9361_ADC_DMA_BASEADDR are not defined. I checked on the xparameters.h file and I see that there is no AD9361 related defined.


Is there problem with the exportation of the project on EDK or anything alse!? How to define on xparameters.h the required addresses!?


Regards,

jetmir

Outcomes