AnsweredAssumed Answered

AD8368 input GAIN voltage ?

Question asked by sss on Aug 5, 2014
Latest reply on Aug 6, 2014 by sss

HI,

 

AD8368 input GAIN(Pin1) voltage range is 0 - 1V.

But,There is no description of the absolute maximum rating for GAIN(Pin1).

 

Considering limiting circuit of the input voltage, but the voltage setting value?

 

Which is the absolute maximum rating, > VGAIN ?

Supply Voltage (VPSO, VPSI) : 5.5 V ?

VGAIN Range+@ : 1+@ V ?

 

thanks,

sss

Outcomes