AnsweredAssumed Answered

Pin state of ADAU1761 in case of Power OFF

Question asked by TomY on Sep 13, 2010
Latest reply on Sep 17, 2010 by JeradL

Hi,

 

To reduce the power consumption, when IC is Power OFF, which state (Hi-Z, High, Low) should it make a pin in the circuit design?
Especially, I want to know the state of the input pin.
Please refer to the attachment file and describe the answer.

 

I will design the hardware circuit considering this information.

 

And, is it possible to show the Pad Block Diagram of each pin?
If Yes, it will be helpful for us.

 

Thanks, TomY

Attachments

Outcomes