AnsweredAssumed Answered

CLK distributer with CML outputs

Question asked by meir.mardechayev@phnx.co.il on Aug 5, 2014
Latest reply on Aug 6, 2014 by Kyle.Slightom

Accubeat, one of my customers, is looking for CLK distributer with CML outputs, and following requirements:

Nubmer of Inputs: 1

Number of outputs: 4

low jitter and low skew performance.

The output clock frequency  range: 1Hz - 2GHz

I saw a AD9540, but it's 1:1, and higher jitter and skew and lower frequency.

 

Can you recommend CLK distributer according to requirements?

Maybe anything soon to be release?

 

Regards,

Meir

Outcomes