AnsweredAssumed Answered

Setting up the communication between zedboard and pc via ethernet cable.

Question asked by Jetmiri on Aug 4, 2014
Latest reply on Aug 8, 2014 by larsc

Dear all,

 

I am using fmcomms2 with zedboard. I am trying to make the data streaming example as it is given in Simulink libiio [Analog Devices Wiki] The problem is that I can not make the board to communicate with my PC. My set up is that I am connecting the zedboard via an ethernet cable with my PC and I am putting both Ip on the same subnet. I am using the IP of zedboard inside the iio_source object. But when I am running the Simulink project as it is given in the upper-mentioned link it gives an error.

 

I should mention that I am using the SD card to set up the linux on zedboard.

 

Am I missing something from the setup or what!? How can I make the communication between zedboard and PC via ethernet cable!?

 

Any help will be appretiated.

 

Thanks in advance,

Jetmir.

Outcomes