AnsweredAssumed Answered

ADP1047 using for DC/DC

Question asked by ehoerner@bron.ch on Aug 4, 2014
Latest reply on Aug 7, 2014 by ncw

Hello,

 

could the ADP1047 be used for DC/DC design? I want to design a SEPIC controller like this one:

 

http://www.analog.com/static/imported-files/application_notes/AN-1126.pdf

 

The requirements are as follows:

 

Vin=12-15V

Iin=20A-40A

Vout=100V-500V

Iout=0.5A-0.8A

 

It wold be nice to use this controller becouse of abbility for adjusting the Vout. If it is possibel, what settings should I make and should I make changes to the hardware?

 

Thanks a lot!

 

Eugen

Outcomes