AnsweredAssumed Answered

CRITICAL WARNING: [IP_Flow 19-664] Failed to create directory 'c:/fmcomms/hdl-master/projects/fmcomms2/zc702/fmcomms2_zc702.srcs/sources_1/bd/system/ip/system_axi_hdmi_clkgen_0/work/c:/FMCOMMs/hdl-master/library/common' to copy 'c:/FMCOMMs/hdl-master/libr

Question asked by psteinke on Aug 1, 2014
Latest reply on Aug 1, 2014 by AdrianC

There are many many critical warnings, and errors (see attached) in the zc702 / fmcomms2 / Vivado 2013.4 build.  I've highlighted a couple below.


Can anyone solve the 'synth_1' failed  issue?


what version of Vivado is correct for fmcomms2?


This is one type of anomolie (critical warning) showing up several times...

CRITICAL WARNING: [IP_Flow 19-664] Failed to create directory

'c:/fmcomms/hdl-master/projects/fmcomms2/zc702/fmcomms2_zc702.srcs/sources_1/bd/system/ip/system_axi_hdmi_clkgen_0/work/c:/FMCOMMs/hdl-master/library/common'           to copy             'c:/FMCOMMs/hdl-master/library/common/up_drp_cntrl.v'         to.



This is the error that stops the build...

[Fri Aug 01 08:45:34 2014] Waiting for synth_1 to finish...

[Fri Aug 01 08:47:34 2014] synth_1 finished

wait_on_run: Time (s): cpu = 00:02:24 ; elapsed = 00:12:15 . Memory (MB): peak = 1102.676 ; gain = 0.000

ERROR: [Common 17-69] Command failed: Run 'synth_1' failed. Unable to open

 

    while executing

"open_run synth_1"

    (procedure "adi_project_run" line 45)

    invoked from within

"adi_project_run fmcomms2_zc702"

    (file "system_project.tcl" line 13)

update_compile_order -fileset sim_1

Outcomes