AnsweredAssumed Answered

SPDIF on EVAL-ADAU1442EBZ

Question asked by guytaar on Sep 10, 2010
Latest reply on Jul 11, 2012 by BrettG

Hi all,

 

I can't make the SPDIF input and/or output work on my EVAL-ADAU1442EBZ. I've made the small project described on the "Quick start guide" which works but when I replace the analog inputs and outputs with SPDIF, it doesn't work. I use the coaxial connectors and the switch is at the correct position. Are there more settings to adjust? I think the clock might have to sync on the input, right? Is there more information (or examples) available for the EVAL-ADAU1442EBZ board?

 

Best regards,

 

Guy

Outcomes