AnsweredAssumed Answered

Sweep mode of AD9834EB Evaluation Board

Question asked by ritula_21 on Jul 30, 2014
Latest reply on Jul 31, 2014 by musach

Im using AD9834 Evaluation Board sweep mode for generating frequencies from 1 MHz to 10 Mhz with an increment of 1 MHZ using single loop and delay of 5000 ms. The output being generated is being fed to my DUT and another to AD8302 as reference. The output of AD8302 is being logged into PC using DAQ. Is there any way out of getting some information from DDS to know when does a particular frequency end? for example some digital bit which indicates the status that informs the end of a particular frequency/ start of new frequency? This will help to differentiate the data logged by DAQ associataed with the frequency?

Outcomes