AnsweredAssumed Answered

[ADV7181D] Do we have to set registers of "Table 22 Recommended User Settings for NTSC" on H/W manual page.137 in our case?

Question asked by Tamu on Jul 30, 2014
Latest reply on Aug 1, 2014 by Tamu

Hello.

I have questions about register setting of ADV7181D.

 

Our use case is as follows:

Input:
   CVBS(NTSC-J) 480i or
   Y/C (NTSC-J) 480i

Output:
  YCbCr 16bit
  HS/VS/FIELD pins are used. (SAV/EAV is not used.)

 

Do we have to set registers of "Table 22 Recommended User Settings for NTSC" on H/W manual page.137 in our case?
I may think the Table 22 settings are required because we use only NTSC-J.
However, there are no descriptions about these registers on the script file.

Do we have to set the Table 22 according to HW manual?
Or can we use the script file without the Table 22 setting?

 

Thank you!
Best regards.

Outcomes