AnsweredAssumed Answered

AD7864 external clock

Question asked by Anderson@ on Jul 28, 2014
Latest reply on Jul 31, 2014 by KarenNE

In the datasheet is not clear for me how to use the external clock.


1-

Do I have to put a 5MHz Crystal? in this case which capacitor values can be used with a 5MHz external crystal oscillator? which crystal parameters are important when using a 5MHz crystal oscillator for proper performance


2- or rather generate a clock signal from a microprocessor?


thank you very much.

Outcomes