AnsweredAssumed Answered

ERROR: [Common 17-69] Command failed: Run 'synth_1' failed. Unable to open

Question asked by psteinke on Jul 24, 2014
Latest reply on Jul 22, 2017 by jones87

I get the following error when running the system_project.tcl script for the 802.11 project for FMComms1/ZC702, and also for FMComms1/ZC702. There are .synth_1 folders in the fmcomms2_zc702.runs and the fmcomms2_zc702.data folders . The folders show up as read only but none of the files are read only. So we have NO IDEA. Please help.

 

     ERROR: [Common 17-69] Command failed: Run 'synth_1' failed. Unable to open

No forums solve this error. I compiled (ran 'source axii_xyz_ip.tcl' ) for all libraries  prior to running the source system_project.tcl command for the project.


Is there a released branch version of the source code from github that builds properly? Does only the latest version fail?


Please help.


Paul

Outcomes