AnsweredAssumed Answered

ADL5390 Minimum Operating Frequency?

Question asked by ripple on Jul 24, 2014
Latest reply on Jul 25, 2014 by jdobler

Hi...


Just wondering if anyone knew if the ADL5390 could be used any lower than the 20 MHz specified in the datasheet.  I saw another product reference that specified 10 MHz as the lowest frequency for the part.  I was wondering if the freq range specified was just a function of the external coupling/matching components or if it was inherent to the IC itself.  I'd like to use it over a range of about 5-50 MHz if possible.

Outcomes