AnsweredAssumed Answered

I have a strange situations with AD9224

Question asked by hallovipin on Sep 9, 2010
Latest reply on Sep 10, 2010 by Georgy

I am trying to interface AD9224 40 MSPS ADC to spartan 3 FPGA. I am generating 12.5 Mhz clock with FPGA and giving it to ADC as a sampling clock.
What I observe that when I am feeding clock to ADC analog signal (which is to be sampled) attached to it gets very noisy.
I went for analysis and found that the noise frequency is exactly that of ADC clock frequency. I had separate analog and digital ground which are shortedonly at the supply input.

 

My signal frequency is 40 kHz while sampling clock to the ADC is 12.5mHz.

 

I examined the FPGA clock not much of jitter is there. I totally suspect the analog and digital ground layout pattern. As mentioned by Fvm both have to be shorted directly under the ADC. I had them shorted at supply input. But can this cause such a serious problem. Later I put even a jumper to short both the grounds as near the ADC as possible but that too didnt help.
One more thing I observed that even the supply for ADC is not switched ON..if I simply feed clock to ADC without having supply on..analog input gets noisy. I am using 50 ohm resisters in series with ADC analog input.

 

any comment

Outcomes