AnsweredAssumed Answered

AD9984

Question asked by mickaelsilica on Jul 23, 2014
Latest reply on Jul 24, 2014 by DaveD

Mu customer is using AD9984 in their design for the YUV input . the product must run with all reader in the market but the rules of the norms are not always applied , and the image can be shift  of some pixels ( vertacl and horizintal ) .  THey want to sync the image in all case by using the Black present in the synchro and the blanking . But they have some problems to sync the active image when the image is Black ( or border is black) .

 

so   Is it possible  with the AD9984 connected to a FPGA  to do a system  to in order to have a system to sync the image when the image are “normal” ou  when they are black ?

thanks

mickael



 

 

 

 

 

 

Outcomes