AnsweredAssumed Answered

Substituting ADL5387 for ADL5382 in CN-0062

Question asked by ELADI on Sep 8, 2010
Latest reply on Oct 8, 2010 by ELADI

If ADL5387 is substituted for ADL5382 in CN-0062, can resistor RCM be used to set common mode input voltage for AD9262 ADC?

Does the 91mA current also apply to ADL5387?

Is this assumption with the BIAS pin (pin3) left open or with an Rbias resistor on pin3?

What is the relationship between the BIAS pin and the current level on pin 18?

How much does the 91mA vary across devices?

Outcomes