AnsweredAssumed Answered

The system is crashed, I can't set anything. And I click the tap on the oscilloscope, it doesn't response.

Question asked by ADI_Wei on Jul 22, 2014
Latest reply on Jul 22, 2014 by rgetz

I used the ZedboardRev.C+AD-FMCOMMS2-EBZ to test.

Download the images at below link, and follow the instructions to write the file to your 8 Gig SD card.

http://wiki.analog.com/resources/tools-software/linux-software/zynq_images

 

Setting up the hardware (ZED) according to the steps listed at below link,

http://wiki.analog.com/resources/eval/user-guides/ad-fmcomms2-ebz/quickstart/zynq

 

After booting from the SD card, open a terminal by using “Ctrl+Alt+T”,

Type “su”, enter

Type the password “analog”, enter

Type “osc”, enter

 

Then I can see another “ADI IIO oscilloscope”

 

But the system is crashapp:addword:crashed, I can't set anything. And I click the tap on the oscilloscope, it doesn't response. I don't know why. This phenomenon happens after I connect the Zedboard to internet. Before that I click the tap normally and set normally.

20140722_150737.jpg

Outcomes