AnsweredAssumed Answered

PLL Lock Question

Question asked by johngrantuk on Jul 21, 2014
Latest reply on Jul 23, 2014 by rbrennan

Hi,

I was hoping someone had some advice on a random question. I have built the circuit in the "Circuit.jpg" attachment using the ADF4159 as the PLL chip. Initially I tested the circuit using a clear wave 1700MHz input as shown in the attached file and the PLL locked and displayed a clean 700MHz IF on the output. Next I changed the input to use a modulated 1700MHz as shown in the final attachment, now the PLL didn't lock and the IF output was constantly drifting in frequency and was very noisy. I realise the modulated signal is a much wider bandwidth signal but could someone explain why this causes the circuit to perform differently and maybe suggest on how to alter it so it can get lock again?

 

Kind regards,

 

John

Outcomes