AnsweredAssumed Answered

IIO runtime error: Unable to create context

Question asked by brandonj on Jul 18, 2014
Latest reply on Jul 18, 2014 by mhennerich

I tried running the iio-monitor example with my zedboard+fmcomms2, but I'm not having success connecting to the device. I see the curses ui and it prompts me for the server ip/hostname. I changed from localhost to the ip I assigned on the target and press enter, but the application immediately closes. I assume the IIO context is attempting to talk to the iio command server, which appears to be running on the target? When it returns it prints to stdout: "ERROR: Unable to create context: No such file or directory"

 

On the target via serial port the ip is assigned as:

 

analog@linaro-ubuntu-desktop:~$ ifconfig

eth2      Link encap:Ethernet  HWaddr 00:0a:35:00:01:22 

          inet addr:192.168.1.2  Bcast:192.168.1.255  Mask:255.255.255.0

          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

          RX packets:59 errors:0 dropped:0 overruns:0 frame:0

          TX packets:131 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

          RX bytes:25613 (25.6 KB)  TX bytes:19769 (19.7 KB)

          Interrupt:54 Base address:0xb000

 

I can successfully ping from the host:

 

azure@azure-OptiPlex-790:~/work/libiio/examples$ ping 192.168.1.2

PING 192.168.1.2 (192.168.1.2) 56(84) bytes of data.

64 bytes from 192.168.1.2: icmp_req=1 ttl=64 time=0.457 ms

64 bytes from 192.168.1.2: icmp_req=2 ttl=64 time=0.357 ms

64 bytes from 192.168.1.2: icmp_req=3 ttl=64 time=0.377 ms

64 bytes from 192.168.1.2: icmp_req=4 ttl=64 time=0.345 ms

^C

--- 192.168.1.2 ping statistics ---

4 packets transmitted, 4 received, 0% packet loss, time 2999ms

rtt min/avg/max/mdev = 0.345/0.384/0.457/0.043 ms

 

IIO server is running?

 

analog@linaro-ubuntu-desktop:~$ ps -aef | grep iio

root      1546  1526  0 00:00 ?        00:00:00 /bin/nc -l -l -p 1234 -e /usr/local/bin/iio_cmdsrv

analog    2627  2563  0 01:20 ttyPS0   00:00:00 grep iio

 

Any ideas? Thanks

Outcomes