AnsweredAssumed Answered

[BD 5-216] error in [building the project in Vivado]

Question asked by woong.lee on Jul 16, 2014
Latest reply on Sep 13, 2016 by CsomI

Currently i'm using zc702 + fmcomms3 and Vivado 2014.2, ISE 14.7

 

I met an error  following the instruction of Building on Vivado    [Analog Devices Wiki]

 

the error message is :

 

ERROR: [BD 5-216] VLNV <xilinx.com:ip:processing_system7:5.3> is not supported for this version of the tools.The latest version is:5.4

ERROR: [Common 17-39] 'create_bd_cell' failed due to earlier errors.

 

 

    while executing

"create_bd_cell -type ip -vlnv xilinx.com:ip:processing_system7:5.3 sys_ps7"

    invoked from within

"set sys_ps7  [create_bd_cell -type ip -vlnv xilinx.com:ip:processing_system7:5.3 sys_ps7]"

    (file "../../../projects/common/zc702/zc702_system_bd.tcl" line 27)

 

 

    while executing

"source $ad_hdl_dir/projects/common/zc702/zc702_system_bd.tcl"

    (file "system_bd.tcl" line 2)

 

 

    while executing

"source system_bd.tcl"

    (procedure "adi_project_create" line 94)

    invoked from within

"adi_project_create fmcomms2_zc702"

    (file "./system_project.tcl" line 7)

 

 

I built the project file which is in \hdl\project\fmcomms2\zc702\system_project.tcl after building every .tcl files in library.

 

the message above shown up again even after clean \hdl folder and re-building libraries.

 

I"V SEARCHED FOR SOLUTION https://ez.analog.com/thread/42721

and followed rejeesh's guide.

"add ip" - "ZYNQ7 Processing System" (its' vlnv is xilinx.com:ip:processing_system7:5.4) ,

the Tcl Consol shows :

startgroup

create_bd_cell -type ip -vlnv xilinx.com:ip:processing_system7:5.4 processing_system7_0

create_bd_cell: Time (s): cpu = 00:00:08 ; elapsed = 00:00:08 . Memory (MB): peak = 623.703 ; gain = 15.113

endgroup

 

and ZYNQ Processing System is added to Diagram Diagram.PNG

 

 

what should i do more to process it completely? (and see a SDK_Export folder which should be created in ../fmcomms2_board.sdk/SDK ?)

Outcomes