AnsweredAssumed Answered

FMCOMMS4-EBZ max. sample rate

Question asked by mtb-guy on Jul 14, 2014
Latest reply on Jul 18, 2014 by mhennerich

I'm presently using the AD-FMCOMMS4-EBZ with a ZC706 and would like to configure it for the maximum supported ADC rate, which based on the AD9364 Reference Manual (UG-673) should be 122.88 Msps.  I'm using the reference design with the iio-based osc utility but it does not allow me to set this rate (maxes out at 61.44 Msps).  I've attempted to manually manipulate settings using the iio file system-based device driver in an attempt to overcome this limitation but have not been successful.  Can you illustrate a short procedure for setting up the demo design for a sample rate of 122.88 Msps?

Outcomes