AnsweredAssumed Answered

ADXL345 characterization data at 3.3V power supply is available?

Question asked by Jane on Jul 13, 2014
Latest reply on Jul 21, 2014 by venkat

Dear Sir,

I have a question regarding ADXL345 operation voltage. It specifies 2.0 V to 3.6 V.

In the datasheet, ADXL345 is tested and specified at a supply voltage of VS = 2.5 V; however, it can also be powered with 3.3 V.

It is said the performance parameters will change with Vs: offset, sensitivity, noise, self-test, and supply current.

Is it possible to supply the ADXL345 characterization data at 3.3V power supply?

The performance parameter is better or worse at 3.3V power supply?

 

Best Regards,

Jane

Outcomes