AnsweredAssumed Answered

ADAS1000 Power Supply Adapter

Question asked by tapanshahp on Jul 10, 2014
Latest reply on Jul 15, 2014 by CatherineR

Hi,

Today when I was trying to use the ADAS1000 Eval Kit and I plugged in the supply adapter I saw "smoke"! The diode D9 blew up and now is all charred up! I have a spare diode that I can replace it with.

 

I want to make sure that the adapter that I am using is the one for this board so that this doesn't happen again.

 

AC/DC ADAPTER

TYPE: FW7660M/05

Input: 100-240V

50-60Hz/ 205-110mA

Output: 5V / 1.6A

 

Manufacturer is: FRIWO

 

Please confirm so that after I replace the diode i can still use the Eval Kit.

Thanks,

Tapan.

Outcomes