AnsweredAssumed Answered

How to amplify the signal output UG-032

Question asked by anaptrs@gmail.com on Jul 10, 2014
Latest reply on Jul 14, 2014 by anaptrs@gmail.com

Dear

 

I need help to make a specific application with development kit the Evaluation Board User Guide UG-032.

I need to increase the signal intensity by up to 110dB, this is made possible in sigmastudio using a second-order filter Medium Size Eq, but the hardware does not support, because their outputs are limited by their reference voltage amplifiers in 2.5 V, because the circuit power.

I wonder if there is any extension board or another type of amplifier that can be connected allowing for the increase of the signal level up to 110dB.

 

Thank you!

Outcomes