AnsweredAssumed Answered

VF Converter

Question asked by wallman16 on Jul 7, 2014
Latest reply on Jul 8, 2014 by JohnnyG

Hi ,

 

Is there any solution for Output frequency @ 5 Mhz . AD7741 max output frequency is rated at 3072kHz but would like to

 

I  read the following thread and seems like AD7741 cannot be used to output 5 Mhz .

The solution of over 3MHz output with AD7741

 

Do you have any other ways to convert voltage to frequency conversion , Input range +/-15V.

 

Thanking you

With best regards and wishes

Outcomes