AnsweredAssumed Answered

Running the LCD and Audio loop back at the same time.

Question asked by ErangaW on Jul 7, 2014
Latest reply on Jul 9, 2014 by CraigG

Hey I am trying to combine two functions for the AD-SP BF548 ,the LCD and the AUDIO CODEC functionality. I am doing this by altering the sample code file Audio_Loopback. To the project file source files section I added LCD.c and too the headerfiles section i added LCD.h. When trying to compile the project it results in the following error.

 

"..\..\..\Getting Started Examples\Common\LCD.c", line 161: cc0020:  error:

          identifier "adi_dcb_QueueHandle" is undefined

          DCBQueueHandle = adi_dcb_QueueHandle;

                           ^

 

 

1 error detected in the compilation of "..\..\..\Getting Started Examples\Common\LCD.c".

cc3089: fatal error: Compilation failed

Tool failed with exit/exception code: 1.

Build was unsuccessful.

 

 

 

What is the proper way i should go about added the two functionality's together provided by the example code.

 

My end goal of the project is too have a lcd display which when you press allows the code within the audio_loopback.c file to process in the input audio to do voice recognition. Coding this all in VisualDSP++ 5.1.

 

Cheers
Eranga

Outcomes