AnsweredAssumed Answered

ADP1046A-100_EVALZ

Question asked by ncw on Jul 3, 2014
Latest reply on Jul 10, 2014 by james.xie


Dear Sir,

 

I want to modify the ADP1046A-100_EVALZ to get the 24Vin, 5Vo/6A.

I change the R10 of main board from 10ohm to 20ohm, and R5/R7/R10 of Daughter card from 11Kohm to 4Kohm, and R1 of Daughter card FROM 27Kohm to 12Kohm.

 

And  below is some questions.

 

1. The Vin in GUI monitor just around 10V in the no load.

2. The Vin slow increase based on the load increase, but only up to 21V(It should be 24V).

 

Could you please advise the root cause?

Thanks.

 

Best regards

 

NC

Outcomes