AnsweredAssumed Answered

Two ethernet port conflict on BF609

Question asked by LuigiDiPalo on Jul 2, 2014
Latest reply on Jul 23, 2014 by VineethaThomas

Hi,

I've a problem with my custom board.

I've realized a board with two ethernet port, two different DP83848, one for each core.

The firmware fot the 2 core are identical but only with a different configuration of ip addrress and ethernet port used.

If I work only with the first core, all works fine. If I enable the second core, the net of the first stops to work and the second net never start!

If I run in debug both the cores say that are connected to the net but i'm also not able to ping them.

Attached stays the firmware!

Attachments

Outcomes