AnsweredAssumed Answered

[ADV7611] ABSOLUTE MAXIMUM RATINGS of "SCL/SDA Data Pins to DVDDIO" on datasheet P.7.

Question asked by Tamu on Jul 2, 2014
Latest reply on Jul 3, 2014 by Tamu

Hello,

I have a question about ABSOLUTE MAXIMUM RATINGS of ADV7611.

There is a following description about ABSOLUTE MAXIMUM RATINGS of "SCL/SDA Data Pins to DVDDIO" on datasheet P.7.
--------------------------------------------
Parameter
 SCL/SDA Data Pins to DVDDIO
Rating
 DVDDIO − 0.3 V to DVDDIO + 3.6 V
--------------------------------------------

 

Is the "DVDDIO + 3.6 V" correct?
When DVDDIO is 3.3V, it indicates ABSOLUTE MAXIMUM RATINGS is from 3.0V to 6.9V.
I think the "DVDDIO + 3.6 V" is not right and the "DVDDIO + 0.3 V" is right.
What do you think?

 

Thank you.
Best regards.

Outcomes