AnsweredAssumed Answered

One question for your AD8330

Question asked by Kaos on Jul 1, 2014
Latest reply on Jul 9, 2014 by Kaos

Dear Sir/Madam,

 

As for your good AMP AD8330,
Your datasheet page-3 show as
"Full-Scale Input, when VDBS=0V, and differential drive, min.±1.4V."
So can I use by the input signal 1.0V-3.5V (peak to peak) biased 2.5V center?
We will amplify this to 0.5V-4.0V.
I think that it is OK if I adjust the gain by Vmag and Vdbs, correct??

Also I note fig-49 on page-16 your datasheet for this incident.

 

Thanks Kaos

Outcomes