AnsweredAssumed Answered

Build FMCOMMS2 reference design on Vivado 2013.4

Question asked by LakshmiS on Jun 25, 2014
Latest reply on Jun 25, 2014 by mhennerich

Has anyone sucessfully build the FMCOMMS2 reference design on Vivado 2013.4? I am able to build the libraries by running the TCL script " source ./axi_ad9361_ip.tcl". But, am not able to create a board design in IPI. I am getting the following error (version mismatch) when I try running the script "source ./system_project.tcl" for fmcomms2/zc706. Does the reference design (shared at https://github.com/analogdevicesinc/hdl) work on Vivado 2013.4?

 

 

ERROR: [BD 5-216] VLNV <analog.com:user:axi_dmac:1.0> is not supported for this version of the tools

ERROR: [Common 17-39] 'create_bd_cell' failed due to earlier errors.

 

    while executing

"create_bd_cell -type ip -vlnv analog.com:user:axi_dmac:1.0 axi_ad9361_dac_dma"

    invoked from within

"set axi_ad9361_dac_dma [create_bd_cell -type ip -vlnv analog.com:user:axi_dmac:1.0 axi_ad9361_dac_dma]"

    (file "../common/fmcomms2_bd.tcl" line 37)

 

    while executing

"source ../common/fmcomms2_bd.tcl"

    (file "system_bd.tcl" line 3)

 

    while executing

"source system_bd.tcl"

    (procedure "adi_project_create" line 94)

    invoked from within

"adi_project_create fmcomms2_zc706"

    (file "./system_project.tcl" line 7)

 

Thanks,

Lakshmi

Outcomes