AnsweredAssumed Answered

max length of buffer to copy data from RAMDisk

Question asked by akash4488 on Jun 24, 2014
Latest reply on Jul 22, 2014 by CraigG

I am enumerating the external RAM as a USB mass storage device on a customised BF548 board,however when i want to copy the data from the specific RAM memory location(the address from where the data storage starts) into a u8 array of size 100000,then only the first 36000 places in the array contain the data and the other places are empty(the size of data in the RAM storage is more than 4MB so i have enough data to fill the u8 array).Can anyone suggest any workaround so that all the 100000  locations in the u8 array are filled with data.

Outcomes