AnsweredAssumed Answered

Which ADC Board to use for wide Bandwidth RF Signal?

Question asked by SDR on Jun 23, 2014
Latest reply on Jun 23, 2014 by charlyelkhoury

I have a 160 Mbit modulated OQPSK signal having a bandwidth of 132 MHz (80 MHz*1.65 Roll-Off) at 720 MHz RF.

I am Looking for a FMC board to get the I&Q channels to pass to a FPGA carrier card.

I checked the FMCOMMS1-EBZ board which has demodulators and ADC's integrated.

It supports 250 MSPS per channel but I'm not sure if it is suitable for this task.

I am not sure if I Should I use the new AD-FMCADC2-EBZ FMC BOARD which is 2500 MSPS.


Please help...(Knowing what the minimum required sampling rate per channel is would definitely help)

Outcomes