AnsweredAssumed Answered

Suspect IPPOTP in BF51X Datasheet

Question asked by ADI.user on Aug 26, 2010
Latest reply on Aug 30, 2010 by ADI.user

Hi,

pg27 of the latest revision (Rev.0 Jan 2010) of the datasheet for the ADSP-BF51X lists the following:

 

IPPOTP Memory Read     100mA (typ)  under the condition VPPOTP = 2.5V & Tj=25degC

IPPOTP Memory Write        3mA (typ)  under the same conditions !!

 

Wondering if there has been a typo and that it shouldn't be 100uA for the read.

 

Also there is a problem with the conditions for writing in that VPPOTP has to be 6.9 - 7.1V, not 2.5V.

 

Could you please confirm IPP for reading & writing to OTP memory.

 

Thanks

Outcomes