AnsweredAssumed Answered

ADF4360-0 : The VCO output is damping at changing VCO from 2.48GHz to 2.42 in ADIsimPLL.

Question asked by Nikkee on Jun 20, 2014
Latest reply on Jun 25, 2014 by Nikkee

Hi,

 

We have made the simulation of ADF4360-0 using ADIsinPLL in the following conditions as the attached file.
    - Min. Frequency : 2.42GHz
    - Max. Frequency : 2.48GHz
    - Frequency shift : From 2,48GHz to 2.42GHz
   
The result is that the VCO output is damping between 2.56GHz and 2.36GHz in the transient changing from 2.48GHz to 2.48GHz.

The VCO output mute function cannot be used because of our system requirements.

The VCO output cannot be gone out of the ISM band (2400~2500MHz).

Can the VCO output damping be within the ISM band (2400~2500MHz)?

 

Best regards,

 

Nikkee

Outcomes