AnsweredAssumed Answered

Reference design for FMC176 - usage with FMC230

Question asked by 8Strings on Jun 18, 2014
Latest reply on Jul 11, 2014 by 8Strings

Hello,

 

I have a question concerning the reference design for FMC176. On the documentation I was reading that this design can be used also with boards mounting the same DACs such as the FMC230.

We are using working with an FMC160 and an FMC230 mounted on a VC707 board, and I have some doubts on how to use the reference design in our case.

First of all, is it possible to use the AD9129 IP Core to drive two DACs mounted on two different boards? (like in our case, one DAC is on the FMC160 on FMC1, and the other one is on the FMC230 - channel 0 - on the FMC2).

 

After getting the reference design and so the xps project, we have updated a couple of IP cores to the new version (we are working with the version 14.7 of the edk). After this we run into some errors concerning missing files, related to the ip_cores coming with the reference design:

 

ERROR:EDK:1405 - File not found in any repository 'axi_jesd204b_rx4_v1_00_a/hdl/verilog/jesd204b_rx4.v'

ERROR:EDK:658 - BlackBox Netlist file axi_jesd204b_rx4_v1_00_a\netlist/jesd204b_rx4.ngc not found

ERROR:EDK:708 - Can not get list of netlist files for core axi_jesd204b_rx4 1.00.a .

The pcore has a pre-synthesized netlist specified through BBD and the list of parameter combinations listed for the instance in MHS does not match any of the combinations in the BBD.

ERROR:EDK:1405 - File not found in any repository 'axi_ad9129_v1_00_a/hdl/verilog/cf_ddsx_1.v'

ERROR:EDK:658 - BlackBox Netlist file axi_ad9129_v1_00_a\netlist/cf_ddsx_1.ngc not found

ERROR:EDK:708 - Can not get list of netlist files for core axi_ad9129 1.00.a .

The pcore has a pre-synthesized netlist specified through BBD and the list of parameter combinations listed for the instance in MHS does not match any of the combinations in the BBD.

ERROR:EDK:1405 - File not found in any repository 'axi_ad9129_v1_00_a/hdl/verilog/cf_ddsx_1.v'

ERROR:EDK:658 - BlackBox Netlist file axi_ad9129_v1_00_a\netlist/cf_ddsx_1.ngc not found

ERROR:EDK:708 - Can not get list of netlist files for core axi_ad9129 1.00.a .

The pcore has a pre-synthesized netlist specified through BBD and the list of parameter combinations listed for the instance in MHS does not match any of the combinations in the BBD.

 

Is there any solution regarding this problem? What can we do to put the reference design up and working?

 

BR,

Giovanni

Outcomes