AnsweredAssumed Answered

Do ADV7393 and ADV7180 can handle custom PAL resolution?

Question asked by YanEmbrio on Jun 18, 2014
Latest reply on Jun 19, 2014 by DaveD

Hi,

 

Because of some Jitter testing gear limitation, I need to create and use a non-standard: SMPTE 259m Level C resolution: 624i50.

4:2:2, 10bits, 864 samples per line, 25 Frames seconds, but 624 lines by frame (not 625).

 

My questions is:

Do the ADV7393 Video encoder will be able to convert this numerical signal to an analog "custom PAL" standard with 624 lines?

Do the ADV7180 Video decoder will be able to convert this "custom PAL" signal and decode it into his numerical version?

 

Thanks

Outcomes