AnsweredAssumed Answered

Can I use AD-FMCOMMS1-EBZ as a RF front end to test out a CDMA demodulator design?

Question asked by Wing on Jun 18, 2014
Latest reply on Jun 23, 2014 by rejeesh

Hi,

 

I am trying to test out a CDMA demodulator written in VHDL and I am planning to load it onto a Xilinx ML605 evaluation board to test it out.  I think considering using the AD-FMCOMMS1-EBZ as the RF front end for my test and wondering if this will work.

 

The required frequency band is s-band and analog bandwidth is 2MHz to 20MHz.  Will someone give me some insights as to whether this board is what I need to do performance testing for the demod?

 

Also, can AD-FMCOMMS1-EBZ do IF sampling with the ADC instead of baseband sampling?

 

Thanks,

Wing

Outcomes