AnsweredAssumed Answered

CFR using the AD9361

Question asked by FreddyS on Jun 17, 2014
Latest reply on Jun 18, 2014 by tlili

Hello,

We would like to implement CFR using the AD9361 and we would like to test it on 10MHz WiMAX signal.

I have few questions:

   

  1. Can we use the AD9361 as shown in the attached file.  Tx sample clock = 44.8MHz and Rx sample clock = 11.2MHz ?
  2. Why we get an error message “ADC CLK min = 10.5MHz, max = 672MHz” ? (Our ADC clock is 268.8MHz)

imageFile.jpg Thanks a lot

Freddy    

Outcomes