AnsweredAssumed Answered

Updating PL+Linux boot image for zedboard+FMCOMMS2 remotely?

Question asked by apillai2011@gmail.com on Jun 16, 2014
Latest reply on Jun 17, 2014 by larsc

Hi,

 

I am using the Zedboard with FMCOMMS2 with the BOOT.BIN + Linaro loaded on to 2 partitions of an SD card. I am doing an iterative develop-build-test cycle with the Linux kernel (playing with the driver), and was wondering if it was possible to update the BOOT.BIN remotely (i.e. without physically removing the SD card, mounting the boot partition, overwriting it, and then putting it back in the Zedboard). Apart from improving dev cycle efficiency, it would also be preferable to avoid the mechanical issues of manipulating the board repeatedly.

 

Thanks,

Arun

Outcomes