AnsweredAssumed Answered

AD9361 FMC cards - external ref clock option

Question asked by obalaj Employee on Jun 12, 2014
Latest reply on Jun 18, 2014 by obalaj

Hi,

 

In order to provide an external ref_clk,  do we need to depopulate the 40MHz crystal oscillator or can we simple input a signal on SMA connector (30.72 MHz).

We upgraded the FPGA code using the upgrade all from Xilinx and we seem to have issues with the HDMI.  A few of the cores
have newer versions in 2014.1 and I don’t know if this is causing the issue.  Is there a release of the design for 2014.1?  Is there a fix
for the HDMI that I should need?

 

Thanks

Ovidiu.

Outcomes