AnsweredAssumed Answered

HCC Embedded Flash Translation Layer License

Question asked by akash4488 on Jun 10, 2014
Latest reply on Jun 10, 2014 by CraigG
Branched from an earlier discussion

Hi Martin,

I am working with a customised board based on BF548 and having a micron 2gb nand flash ,64mb ram and usb otg.

When i run the USB mass storage example (which is there in the VISUAL dsp++ 5 sofwtare) and i have made the following configurations in the code as follows

 

#define _USE_ONBOARD_PERSISTENT_MEDIA in mass_storage_app.c

 

 

and

 

#define DEVICE_TYPE DEVICE_NAND

i bsp_bf548.c

 

then it gives the following error

 

IT fails at the following line in mass_storage_app.c

 

 

/* If HD is NOT connected to this board */
       if (Result == ADI_DEV_RESULT_SUCCESS)
{printf("\nsucess to Register the PID with the class driver");}
     if(Result != ADI_DEV_RESULT_SUCCESS)
    {
        failure();
    }

 

 

and the error is

 

 

!!!! A valid license has not been found !!!!

    Please contact HCC Embedded (www.hcc-embedded.com) to arrange a license.

 

 

I would be helpful if you can please tell a workaround to overcome this problem

 

Outcomes