AnsweredAssumed Answered

DC power consumption in sleep, wait, and alert modes in AD9361

Question asked by JeffGoos on Jun 9, 2014
Latest reply on Jun 19, 2014 by JeffGoos

I've measured the DC current consumption at the 3V3P point on the FMcomms2 evaluation board by removing L302.  I'm using the AD9361 in TDD mode and using all defaults provided by the latest IIO interface software as of today. 

 

Sleep = 9mA.

Wait = 80mA.

Alert = 80mA.

 

Two questions.

1) Do these current measurements seem correct?  I expected Wait mode to be lower than Alert.

2) What exactly is on and off in Sleep, Wait, and Alert modes?  Which application document best defines these modes?

 

Thanks.

Outcomes