AnsweredAssumed Answered

Questions about 9984A

Question asked by StevenWeyrich on Jun 5, 2014
Latest reply on Jun 5, 2014 by DaveD

Hi,

I've two questions to the AD9984A:

 

1. This IC however has a 10 bit output, but it might possible be converted to 8 bit as needed by the TFT display by adjusting the gain and/or offset registers of the AD9984A?


2. Do you know if the AD9984A is able to receive a resolution as low as 480x272 and what the output clock speed would be in this case?

 

The Application is to use a 4.3" FTF Display with DVI/VGA/DisplayPort. But it is only capable to work with 12 MHz.

So far can I downstreem the DVI/ Displayport Data to a lower data rate?

Thanks!

Outcomes