AnsweredAssumed Answered

Degbu ARM application for ZED+AD-FMCCOMMS2-EBZ

Question asked by bemiki@gmail.com on May 31, 2014
Latest reply on Jun 1, 2014 by bemiki@gmail.com

Hi all,

I recently installed AD SD image on a ZED board with AD-FMCCOMMS2-EBZ

I cannot debug application using  the Remote ARM debug application within the Xilinx SDK

 

any suggestion ....

 

BR

MIKI

 

--- error message ----

(gdb)

10-target-select remote 10.0.0.16:1234

10^error,msg="10.0.0.16:1234: A connection attempt failed because the connected party did not properly respond after a period of time, or established connection failed because connected host has failed to respond."

(gdb)

11-gdb-exit

11^exit

 

(the debug work when using the Xilinx SD image)

Outcomes