AnsweredAssumed Answered

AD9361 & AD9364 I/Q Sample Rate

Question asked by Enrico on May 30, 2014
Latest reply on Jun 4, 2014 by Enrico

We are evaluating AD9361 or AD9364 to replace current radio front end of an existing SDR platform.


Assuming:

- two bidirectional channels working in parallel

- all internal filtering bypassed and data from/to digital interface going straight to the A/D,D/A converters

- full duplex operation mode


I understand that:


a) If we use a single AD9361, the maximum operating sampling rate can be 30.72 Ms/s

b) If we use two AD9364, the maximum operating sampling rate can be 61.44 Ms/s


The lower sampling rate in case of AD9361 is coming from the two multiplexed channels on the same digital interface.

 

Do you confirm it ?

 

Thanks in advance,

Enrico

Outcomes