AnsweredAssumed Answered

CVT-ADC-FMC-INTPZB with AD9268-125EBZ on Zynq?

Question asked by flambda on May 28, 2014
Latest reply on May 28, 2014 by rejeesh

Hi,

 

I like to connect a AD9268-125EBZ to my Xilinx Zynq via FMC.

It seems that we CVT-ADC-FMC-INTPZB interposer card could be used for this.

So my question is, are they combatible?

I have already found multiple similar questions so sorry if I am asking something obvious here.

 

There is this:

http://ez.analog.com/message/82028#82028 but I am unsure if this is due to a problem with the interposer and the AD9268

or due to the ZED.

My guess is it is due to the ZED as the AD9269 eval board, which should be compatible with the AD9268 eval board, does not seem to have this problem (see here: http://ez.analog.com/message/88395#88395)

 

So my question stands:

Can I use the CVT-ADC-FMC-INTPZB with AD9268-125EBZ on Zynq?

 

With best regards,

 

flambda


Outcomes