AnsweredAssumed Answered

About ADL5511-EVALZ

Question asked by yuji on May 26, 2014
Latest reply on May 27, 2014 by enash

There were the following questions from our customers.

 

It is measured by the following configurations in ADL5511-EVALZ.

 

SG-RFIN-ADL5511-VENV-multimeter

 

Vpos:5V

Temperature:25℃

InputFrequency:2.45GHz(No modulation)

Input level:-25dBm

 

 

1.It is assumed that the voltage of 0.01V following is output from "VENV," but 1.1V is output.

  Does this would have been determined to be no signal?

 

2.Will it not work properly even if you enter the sine wave to this board?

 

3.Are there any possible causes else?

 

Regards,

yuji

Outcomes