AnsweredAssumed Answered

ADAU1442 - Can I output two TDM16 streams?

Question asked by mike-gr on May 22, 2014
Latest reply on May 22, 2014 by mike-gr

I'm processing 16 stereo channels. Can I output those as two TDM16 streams using the ADAU1442? I think the answer is no, because there aren't enough output channels.

 

I also want to verify I can input two TDM8 streams. That shouldn't be a problem, just the number of outputs.

 

I'm just making sure I didn't overlook something, so I appreciate a confirmation on the TDM16 outputs.

 

Thanks everyone!

Outcomes