AnsweredAssumed Answered

AD9388A ESD protection

Question asked by HankZ on Aug 18, 2010
Latest reply on Aug 18, 2010 by HankZ

A question generated from customer support:

 

In accordance with the Absolute Maximum Rating System (IEC 60134):

  1. what is the maximum value of the input pins’ (TMDS and DDC) contact and air electrostatic discharge voltage bye the IEC 61000-4-2 ESD test?
  2. what is the maximum value of the input pins’ (TMDS and DDC) contact and air electrostatic discharge voltage bye the MIL-STD-883 Method 3015 (human body model) test?
  3. do you recommend using an ESD protection IC on the inputs?
  4. If yes, which one do you recommend?

Outcomes